Can't set pin USB_H_DATA on i.MX6 SoloX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't set pin USB_H_DATA on i.MX6 SoloX

545 Views
user1391
Contributor I

Hello everyone,

we are trying to set pin USB_H_DATA (GPIO7 IO 10) but are unable to do so.

We tried it with 'gpioset /dev/gpiochip6 10=1' but reading back the pin always gives zero.

Also, the pin stays at 0 V.

Additionally, we tried it both via device-tree and from within u-boot.

Other GPIOs on the same bank seem to work, except for USB_H_STROBE.

Do you have a suggestion on what is going wrong here?

Thank you very much,

Maik

Labels (1)
0 Kudos
1 Reply

464 Views
igorpadykov
NXP Employee
NXP Employee

Hi Maik

this may be hardware error, connections with other signals, one can

check board layout and perform x-ray screening. May be useful to attach jtag

and toggle gpio, run bare metal test below:

rt-thread/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/gpio at master · RT-Thread/rt-thread · GitHub 

Regarding "USB_H_DATA (GPIO7 IO 10)" one can recheck:

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos