Can't play video using gstreamer 1.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't play video using gstreamer 1.0

2,408 Views
ralph__
Contributor IV

I'm trying to play an MPEG4 video back using gstreamer-1.0 (having moved on from 0.10) but am having trouble with the command line:

# gst-launch-1.0 filesrc location=/usr/sample1080p30_40Mbps.mp4 typefind=true ! qtdemux ! imxvpudec ! queue max-size-buffers=3 ! imxipuvideosink

Setting pipeline to PAUSED ...

[INFO]  Product Info: i.MX6Q/D/S

Pipeline is PREROLLING ...

ERROR: from element /GstPipeline:pipeline0/GstQTDemux:qtdemux0: GStreamer encountered a general stream error.

Additional debug info:

qtdemux.c(4434): gst_qtdemux_loop (): /GstPipeline:pipeline0/GstQTDemux:qtdemux0:

streaming stopped, reason not-linked

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

Freeing pipeline ...

Any ideas what this error is about?  The equivalent command line worked fine on gstreamer-0.10.

Thanks, Ralph.

0 Kudos
Reply
1 Reply

1,391 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ralph

for gstreamer-1.0 commands one can refer to sect.7.3.1.2 Video-only

playback attached Linux Guide, use

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply