I use below codes to open "/dev/block/mmcblk0" in android kernel:
static const char *filename = "/dev/block/mmcblk0";
static const int  offset = 26623 * 512;
static int emmc_read(void)
{
 mm_segment_t fs;
 struct file *fp = NULL;
 loff_t pos = 0;
 u8 header[512], *data=NULL, *udata=NULL, *vp;
 int len, outlen=0, n, i, ret = -1;
 char *p;
printk("loading file: %s\n", filename);
 fs = get_fs();
 set_fs(KERNEL_DS);
 fp = filp_open(filename, O_RDONLY, 0);
 if (IS_ERR(fp)) {
  fp = NULL;
  ERR("Could not open  file\n");
  goto err2;
 }
....
}
but it failed,it shows below error:
loading file: /dev/block/mmcblk0
Could not open file
Can you tell me how to open "/dev/block/mmcblk0" in android kernel ?
Thanks.
 PeterChan
		
			PeterChan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I used similar code but I don't experience such problem in Android. However, the Android BSP release is r13.5.
Please add the below lines to imx50_rdp/init.rc and try again.
# enable mmcblk0 read by system
chmod 0660 /dev/block/mmcblk0
 
					
				
		
your question interests me.
mmcblk0 is a block device, if you doesn't have mmcblk0pX means this emmc block even not been partitioned.
and I'm curious, is it possible that user space program could/should do operations on this block device?
I stored the files in address "26623 * 512",so I only need to open the "/dev/block/mmcblk0" for read the file contents,
I had made the following test.
1.Add the node of drivers;
    
static int emmcvalue=0;
static ssize_t show_emmc(struct device *dev,
struct device_attribute *attr, char *buf)
{
return snprintf(buf, PAGE_SIZE, "%d\n", emmcvalue);
}
static ssize_t set_emmc(struct device *dev,
struct device_attribute *attr, char *buf, size_t count)
{
int value = simple_strtol(buf,NULL,0);
printk(" value =%d\n",value);
///check the value
if(value ==1)
emmc_read();
emmcvalue = value;
return count;
}
static DEVICE_ATTR(emmc, S_IWUSR | S_IRUGO, show_emmc, set_emmc);
2.When the devices bootup, I call the "emmc" in serial port:
bash-3.2# echo 1 > emmc 
[ 53.799949] value =1
[ 53.802239] loading waveform file: /dev/block/mmcblk0
[ 53.808659] emmc_read,i=4 
[ 53.813369] waveform name: V220_C175_50_WN5331_ED050SC5_BTC.wbf
[ 53.819297] waveform size: 38853
it works well,but I call it in kernel,it can't open. Thanks.
 
					
				
		
I'll suggest using command "dd" to try that if you can retrieve your file or not
.
"dd" command is for write,and I sure the file had been wrote to emmc,because in uboot,I can read the file contents from this address in emmc.
 
					
				
		
if you change your if=, dd can be read, too.
such like "dd if=/dev/mmcblk0 of=/tmp/V220_C175_50_WN5331_ED050SC5_BTC.wbf bs=X seek=X skip=X"
your mean, we can use the dd command to verify whether the file contents exist?but I sure the file is exist,because I can read the file contents in uboot.
 
					
				
		
this also test user space program can access /dev/mmcblk0 or not.
if dd can retrieve your file successfully, that indicate your program might be wrong, or your program just not have the right permission to access /dev/mmcblk0(in this case, sudo sounds a good answer).
I had tested the "dd" command, I think it can't retrieve the file successfully,because when I ran this command in serial port,it didn't have any response:
bash-3.2# dd if=/dev/block/mmcblk0 of=/mnt/sdcard/001.wbf bs=512 seek=26624
Is this command right? How to let dd stop at address ?
 
					
				
		
it won't stop. unless it reach /dev/mmcblk0's end.
you may append count=X to let dd know when it should stop.
for example, bs=512 count=4, dd will dump 512 * 4 = 2048 byte
Can you tell me how to use the dd command to transferred below file contents?
1).When I upgrade the firmware,I use below command to write:
<CMD type="push" body="send" file="files/android/wfname">Sending SoftWare Version</CMD>
<CMD type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=26623 conv=fsync">write software version file to sd card</CMD>
<CMD type="push" body="send" file="files/android/V220_C175_50_WN5331_ED050SC5_BTC.wbf">Sending SoftWare Version</CMD>
<CMD type="push" body="$ dd if=$FILE of=/dev/mmcblk0 bs=512 seek=26624 conv=fsync">write software version file to sd card</CMD>
2),After the devices bootup, I use below command to transferred ,but the results is not the same :
bash-3.2#dd if=/dev/block/mmcblk0 of=/mnt/sdcard/002.txt bs=512 seek=26623 count=1
1+0 records in
1+0 records out
512 bytes transferred in 0.002 secs (256000 bytes/sec)
bash-3.2#
 
					
				
		
dd will dump raw data from input source, and the data you dump is not a "file", it's just a combination of binary strings.
you may need hex editor/viewer to peek the contents of dd's dump file.
on linux, I often using hexdump.
if you using Windows, ultra editor can do this trick.
So, if you wanna retrieve the file you write in mmcblk0, you need:
1. remove the garbage data append in your dd dump. you have to calculate the size, and write a program to retrieve (wait a sec, why not using your previous program, just replace dd file instead /dev/mmcblk0 ? ).
2. or you just format your mmcblk0, and put the file in the file system.
after you get into your system, just mount this mmcblk0pX in /mnt, then get the file
I believe the second one is lot easier.
Thanks for your help,I think we can get the file content from your method,but,it still can't solve my problem,because I need read the wbf file in Eink driver,in funtion "mxc_epdc_fb_init_hw".
If I can't read the wbf file,the Eink driver can't register successful.
From my test,we can run "dd" in serial port,it means,we had the permission to open the "/dev/block/mmcblk0" ?
In android filesystem,the emmc will be divided six partition,and the "/dev/block/mmcblk0" will be stored uboot,kernel, and so on.
bash-3.2# cat /proc/partitions
major minor #blocks name
179 0 3870720 mmcblk0
179 1 2744320 mmcblk0p1
179 2 358400 mmcblk0p2
179 3 1 mmcblk0p3
179 4 40960 mmcblk0p4
179 5 307199 mmcblk0p5
179 6 358399 mmcblk0p6
bash-3.2#
 
					
				
		
Hello,
Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.
For details please see general advice Where to post a Discussion?
Thank you for using Freescale Community.
Thanks for your reminder, I had selected the location as the "i.MX Community",and had selected the catrgory "Android .I.MX50".