Can't include timer.h on i.MX8MQ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't include timer.h on i.MX8MQ?

402 Views
Derek0902
Contributor II

Hi,

I want to write a C program to auto-adjust backlight with ALS, then I need to use timer interrupt to design it.

When I compile the C program, there are no timer.h can be included. How can I add this header file?

 

Regards,

Derek Lin

0 Kudos
Reply
0 Replies