Can't get files from bitshrine.org/gpp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't get files from bitshrine.org/gpp

1,575 Views
evgeniyoparin
Contributor II

Hello everyone! I'm rebuilding rootfs by ltib. So every necessary packet i downloaded with error Error 404: file not found

I can't get files with 'wget' too.

What is wrong?

And can someone give me crashme-2.4.tar.bz2?

Thanks!

Labels (6)
3 Replies

1,351 Views
igorpadykov
NXP Employee
NXP Employee

Hi Evgeniy

you can google this (and any other) package like link below, repack is

to bz2 format (or any suitable) and put in opt/freescale/pkgs directory

crashme-2.4.tar.gz [8037 bytes] - Download Mirrors

Regarding availability files on bitshrine.org it is better to ask them directly.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,351 Views
evgeniyoparin
Contributor II

Igor, thank you for the quick answer!

But i checked this idea before you had answered me, and after that i have another error:

*** No targets specified and no makefile found. Stop.

I downloaded archive, where there are makefile and targets files. But error repeats.

And may be someone have the official crashme-2.4.tar.bz2?

0 Kudos
Reply

1,351 Views
igorpadykov
NXP Employee
NXP Employee

You can check below app note it shows how to add new

package to ltib

pdk2009_12_imx35_Linux_HelloWorld_AN.pdf

IMX35_PDK0912_LINUXDOCS_BUNDLE i.MX35 PDK Linux Documentation Bundle

Regarding "official crashme-2.4.tar.bz2" - all official packages are

already located on Freescale i.MX product web pages.

~igor