Can't get IMX7 to wake from WAIT mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't get IMX7 to wake from WAIT mode

1,079 Views
jordanrh
Contributor II

I can't get IMX7 to wake from WAIT mode, using GPT1 timer as wake source. Cores and SCU are not powered down, and ARM clock is stopped in LPM. This is a clock gated state. I am configuring the system as follows:

GPC_LPCR_A7_BSC = 0x3ff5

 - LPM0 = LPM1 = 1 (WAIT)

 - CPU_CLK_ON_LPM = 0 (turn off ARM clock in LPM)

 - IRQ_SRC_C0 = IRQ_SRC_C1 = IRQ_SRC_A7_WUP = 0 (use IRQ to wake up, masked by IMR0-4)

 

GPC_LPCR_A7_AD = 0x200

 - EN_C0_PUP=1 (enable Core0 power up on LPM exit)

 - L2_PGE=0 (do not power down L2)

 - EN_PLAT_PDN=0 (do not power down SCU)

GPC_LPCR_M4 = 0x80003ff0

  - MASK_DSM_TRIGGER=1

GPC_SLPCR = 0x80000000

 - EN_DSM=1 (enable DSM)

GPC_PGC_ACK_SEL_A7 = 0x80008000

 - Use A7 dummy ack for power down/power up acknowledge

GPC_PGC_C0,C1,SCU[0] = 0

 - do not arm PGC's for power down

GPC_IMR2_CORE0_A7 = 0xFF7FFFFF

 - unmask IRQ 87 (GPT1)

GPT_CR=0x33f

 - use 32khz osc as clock source

 - enable in WAIT, STOP, DOZE, and DBG

I believe the system is entering LPM because

 - power consumption decreases by 120mW. WFI without LPM saves only 60mW

 - If I set LPM=STOP, then screen goes off, which suggests most clocks are stopping, which only happens in LPM=STOP mode

I believe the GP1 interrupt is firing and is properly unmasked because

 - If I do NOT stop A7 clock in LPM, the system resumes from LPM

 - The GPT1 clock gate is configured to keep running in WAIT mode (CCGR124=0x2)

 - If I don't enter LPM mode, the GPT1 interrupt fires, and I see the ISR run

 - I successfully use GPT1 to wake up from CORE0_OFF state, using IRQ as wakeup source, even when GPT1 interrupt is disabled in the GIC. If I do not unmask this IRQ source in IMR, the core does not wake up, which strongly suggests that IRQ wakeup method is configured properly.

I have tried a lot of different things, including powering down cores and SCU, and various configurations of the WUP bits, but I cannot get system to resume from this state.

Any ideas why system isn't waking up?

Labels (1)
0 Kudos
2 Replies

696 Views
jordanrh
Contributor II

IMX7 does have wait mode. It's used by the linux cpuidle driver (./arch/arm/mach-imx/cpuidle-imx7d.c)

I got this to work. I had to set the following things:

 - assign mega/fast mix to A7 domain (GPC_PGC_CPU_MAPPING)

 - enable A7 fast wakeup wait mode (BM_SLPCR_EN_A7_FASTWUP_WAIT_MODE)

 - disable memory low power mode (BM_GPC_MLPCR_MEMLP_CTL_DIS)

These flags are not covered in the datasheet examples. Might want to add them.

0 Kudos

696 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jordan

i.MX7D processor supports low power modes described in
sect.5.1.4.4 Power Modes i.MX7D Reference Manual
http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf

Table 14. Power modes i.MX7D Datasheet
http://cache.nxp.com/files/32bit/doc/data_sheet/IMX7DCEC.pdf

Use cases and software examples described in sect.4.1. Low-power mode use cases
AN5383 i.MX 7DS Power Consumption Measurement
https://www.nxp.com/docs/en/application-note/AN5383.pdf

Software register settings one can find in linux driver sources
(linux//arch/arm/mach-imx/suspend-imx7.S), please look at
Chapter 21 Low-level Power Management (PM) Driver attached Linux Manual and
description in AN5383 app note.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos