Can't find PMIC:PFUZE100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't find PMIC:PFUZE100

1,974 Views
YoshihisaSaitou
Contributor I

Hi,

processor:   MX6Q;

Board     :   SabreAI rev.A

BSP:      :   L4.9.11_1.0.0 (Build by myself) 

                     L4.9.11_1.0.0 (Download demo file)

                    L3.14.52 (Download demo file)

I started it with the above configuration.
However, the following error occurred.
How can I solve it?
Is the board broken?

=======

Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Dec 05 2015 - 02:02:30)

CPU: Freescale i.MX6Q rev1.2 at 792 MHz
CPU: Temperature 25 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 2 GiB
Can't find PMIC:PFUZE100
initcall sequence 8ff8e124 failed at call 178036b0 (err=-19)
### ERROR ### Please RESET the board ###

=======

Best regards,
Yoshihisa Saito

Labels (3)
0 Kudos
4 Replies

1,186 Views
joanxie
NXP TechSupport
NXP TechSupport

how did you download demo image? which .vbs file you do you use? let me check it

0 Kudos

1,186 Views
YoshihisaSaitou
Contributor I

Dear Joan Xie,

Thank you for your reply.

I am not using MFGtool.
I wrote down below.

$ sudo dd if = u-boot.imx of = / dev / sdb bs = 512 seek = 2
$ sync

The board now works once every four times.
Perhaps, I think there is a problem of contact failure.


Best regards,
Yoshihisa Saito

0 Kudos

1,186 Views
joanxie
NXP TechSupport
NXP TechSupport

did you Partitioning the SD card successfully? I couldnt reproduce this issue, maybe you can try to mfgtool, for dd command, don't forget partitioning the SD card and format the card first, and I try the command as below:$ sudo dd if=<U-Boot image> of=/dev/sdx bs=512 seek=2 conv=fsync

0 Kudos

1,186 Views
YoshihisaSaitou
Contributor I

Dear Joan Xie,

Thank you for your reply.

The SD card did the following.

$sudo fdisk / dev / sdb
d [repeat this until no partition is reported by the 'p' command]
n [create a new partition]
p [create a primary partition]
1 [the first partition]
20480 [using the default value will create a partition that starts at offset 2048]
102400 [size of the actual partition = 255 MB]
n [create a new partition]
p [create a primary partition]
2 [the second partition]
122800 [using the default value will create a partition that starts at offset 67584]
<enter> [using the default value will create a partition that uses the remaining space on the card]

w [this writes the partition table to the medium and fdisk exits]

$sudo mkfs.vfat / dev / sdb1
$sudo mkfs.ext 4 / dev / sdb 2

I think that there is a problem because this board has been purchasing a few years ago.
As new information, L3.10.53 works normally.
I have not solved it, but please close .

Best regards,
Yoshihisa Saito

0 Kudos