Hello NXP,
Currently i'm working on i.MX8M Nano EVK Board but while booting it's showing error as :-
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
Training FAILED
Could you please help me ??
Thanks
Nikhil
Solved! Go to Solution.
Hello,
i have the same issue. Can you please explain what exactly has to be done to solve the problem?
Regards,
Lucien
I'm not getting the point of the solution. I'm facing the same issue.
MACHINE=imx8mnevk DISTRO=fsl-xwayland,
bitbake core-image-base
Once I try to boot from the mSD card, I'm getting the same error.
Isn't the Yocto recipe supposed to support i.MX8m Nano EVK as such.
The SD card was written this way:
sudo dd if=tmp/deploy/images/imx8mnevk/core-image-base-imx8mnevk.wic of=/dev/sdd bs=1M conv=fsync
The earlier release worked fine, but once I tried to upgrade to kernel 5.4.24 because reported LDO bug in older one, the new BSP does not boot on target. Some of the images do not even bitbake properly. (Such as fsl-image-machine-test.) I'm confused.
Thanks for quick reply.
i'm able to get booting logs from eMMC through both Tera Term and minicom but while booting from SD Card it's showing an error as :- "Can't find PMIC:PCA9450"
can you please provide any resulting solution ??
Thanks
Nikhil
are you sure that image is the same in eMMC and SD card ?
Best regards
igor
Thanks for quick reply
I didn't flash anything into eMMC. eMMC already contains it's own image while manufacturing the EVK.
I just flashed an image into SD Card. So images might be different in eMMC and SD Card.
Thanks
Nikhil
Hi Nikhil
probably it was wrongly programmed, one can try to reprogram it
using latest Demo Image i.MX 8M Nano EVK
Best regards
igor
thanks for quick reply
I have also tried to flash demo [ Pre-built ] image that you have shared now, but still showing same error. I'm not understanding what to do.
Now, what should be the right solution ??
Please help.
Thanks
Nikhil
so the same image is working differently in eMMC and SD card ?
Best regards
igor
Thanks igor for your support and priceless time.
Your Q :- so the same image is working differently in eMMC and SD card ?
Ans :- NO
I don't know what contains eMMC. but i'm sure that eMMC is having it's own image when i received my Nano Board and then i powerted up Nano board and got boot logs though eMMC. After that i have inserted SD Card into Board and try to get logs but showing that error.
I just flashed image [ imx-image-full ] on SD Card which i have compiled with the help of Yocto User's Guide.
I also tried to flash just U-boot image but still same error.
One of my colleague working on i.MX8M Mini EVK. He is able to get logs both through eMMC [ already present image ] and SD Card [ he has compiled ]. But logs from eMMC and SD Card both are different he said.
Thanks
Nikhil
Hi nikhil29
for "Can't find PMIC:PCA9450" issue one can configure
pmic in ddr script using example on below link and checking signals with oscilloscope:
"Sample configuration in the front of the .ds script for i.MX8MM PMIC configuration'
Best regards
igor
Thanks igor for your kind suppport
Regards
Nikhil