Can't boot from SD0 in i.MX28 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't boot from SD0 in i.MX28 EVK

Jump to solution
2,965 Views
thomaslin
Contributor IV

Hi,

Found a trouble recently. The EVK can't boot by LTIB and Yocto build.

Anyone have idea to fix it?

LTIB-SD.png

LTIB build SD

Undefined Ins.png

Yocto Build error.

Labels (1)
Tags (1)
0 Kudos
1 Solution
2,014 Views
PeterChan
NXP Employee
NXP Employee

It looks something is wrong after change the cpu frequency. In the file ltib/rpm/BUILD/imx-bootlets-src-2.6.35.3-1.1.0/boot_prep/init-mx28.c, would you please define "MEMORY_TEST" and rebuild the boot stream to see if the memory test can pass?

View solution in original post

0 Kudos
12 Replies
2,013 Views
Yuri
NXP Employee
NXP Employee

Have You tried demo images from the Web ?

0 Kudos
2,013 Views
thomaslin
Contributor IV

No, already download it. How to use it?

0 Kudos
2,014 Views
PeterChan
NXP Employee
NXP Employee

The i.MX28 demo image is available at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX28_SW.

After extraction, you should see several .SB and rootfs images. Please follow the instruction in MX28_EVK_Linux_User_Guide.pdf section 5.1.3 to prepare the MMC to boot. This document is also available at the above link.

Please notice that you need to program imx28_ivt_linux.sb instead of imx28_linux.sb since EVK has HAB enabled by default.

0 Kudos
2,014 Views
thomaslin
Contributor IV

Copy imx28_ivt_linux.sb and  imx28_ivt_uboot.sb into ./rootfs/boot
Still get error below

*************************************
$sudo ./mk_mx28_sd /dev/sdb

**************************************

HTLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLLFLC
PowerPrep start initialize power...
Battery Voltage = 4.24V
boot from battery. 5v input not detected
LLLCJan 30 201317:34:07
FRAC 0x92925552
memory type is DDR2
                   Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001
LLLLLLLFLCLLJ
*************************************
$sudo ./mk_mx28_sd -u /dev/sdb

************************************
PowerPrep start initialize power...                                                          
Battery Voltage = 4.24V                                                                      
boot from battery. 5v input not detected
Jan 30 201317:34:07
FRAC 0x92925552
memory type is DDR2
                   Wait for ddr ready 1power 0x00820710
Frac 0x92925552
start change cpu freq
hbus 0x00000003
cpu 0x00010001

0 Kudos
2,015 Views
PeterChan
NXP Employee
NXP Employee

It looks something is wrong after change the cpu frequency. In the file ltib/rpm/BUILD/imx-bootlets-src-2.6.35.3-1.1.0/boot_prep/init-mx28.c, would you please define "MEMORY_TEST" and rebuild the boot stream to see if the memory test can pass?

0 Kudos
2,014 Views
thomaslin
Contributor IV

In bottom of code, I found

*****

    /*Test Memory;*/
    printf("start test memory accress\r\n");
    printf("ddr2 0x%x\r\n", pTest);
    for (i = 0; i < 1000; i++)
        *pTest++ = i;

    pTest = (volatile int *)0x40000000;

    for (i = 0; i < 1000; i++) {
        if (*pTest != (i)) {
            printf("0x%x error value 0x%x\r\n", i, *pTest);
        }
        pTest++;
    }
    printf("finish simple test\r\n");
    return 0;

***********

That mean Test Memory is not ok?

0 Kudos
2,012 Views
PeterChan
NXP Employee
NXP Employee

Yes, I meant to enable this piece of code in boot stream and see if messages "start test memory accress" and "finish simple test" can be shown. Otherwise, your board may have hardware problem.

0 Kudos
2,014 Views
thomaslin
Contributor IV

Only know LTIB build method. If possible to inform me the way to modify?

0 Kudos
2,014 Views
PeterChan
NXP Employee
NXP Employee

Run this command to get the boot stream source code.

$ ./ltib -p boot_stream.spec -m prep

Edit the file ltib/rpm/BUILD/imx-bootlets-src-2.6.35.3-1.1.0/boot_prep/init-mx28.c and add the line "#define MEMORY_TEST".

Run this command to build the boot stream.

$ ./ltib -p boot_stream.spec -f

The imx28_(ivt)_linux.sb and imx28_(ivt)_uboot.sb will be updated.

0 Kudos
2,014 Views
thomaslin
Contributor IV

Dear all,

Thanks, root cause found. EMI_VREF =0V!!

So, check R29 tie to ground in both end. Resolder R29 and the system can bootup now.

Thanks all of your help.

0 Kudos
2,014 Views
PeterChan
NXP Employee
NXP Employee

Hello Thomas,

How many EVKs have you found to have this problem? Have you tried the prebuilt image?

0 Kudos
2,014 Views
thomaslin
Contributor IV

I only have one EVK,

I use 3 kinds pribuild images original Linux image, LTIB prebuild by Ubuntu and Yocto fsl-test image. Test all of them fail.

The pics are fail shown in debug message.

0 Kudos