I tried some basic example code to get a picture from my MIPI camera with OpenCV, but all I get is the following error:
HIGHGUI ERROR: libv4l unable to ioctl S_FMT
HIGHGUI ERROR: libv4l unable to ioctl VIDIOCSPICT
Any hints?
System: Wandboard Quad with Yocto Dora
Camera: e-CAM51IMX6
Access with Gstreamer is working, but only with a low resolution.
Also the same code is working on my dev machine.
Hello Mars Volta,
I have the same issue:
root@nitrogen6x:/usr/bin# DISPLAY=:0 ./camera_test
ov5642_powerdown: powerdown=0, power_gp=0x6
HIGHGUI ERROR: libv4l unable to ioctl S_FMT
HIGHGUI ERROR: libv4l unable to ioctl VIDIOCSPICT
Cannot open initialize camera!
root@nitrogen6x:/usr/bin# ov5642_powerdown: powerdown=1, power_gp=0x6
I did have the camera running via gstreamer on an earlier build on LTIB. The LTIB however had problems building the latest OpenCV source, so I went to yocto and built OpenCV.
The yocto recipes did not include building of gstreamer.
So, I am wondering can you expand on "Use gstreamer to capture frames and feed this to OpenCV"? I think this would be workable for me, but I'm not sure of the method you are suggesting.
Or, alternatively, what is the post-box procedure to have OpenCV work with the Freescale MXC camera interface?
Thanx
Very late reply...
I ran into the same issue when using the wandcam.
I did find that disconnecting the wandcam and plugging in a usb camera (Microsoft Lifecam in my case),
I was able to get video, but I changed the demo program a bit...
#include "opencv/highgui.h
int
main(int argc, char** argv)
{
cvNamedWindow( "Example2", CV_WINDOW_AUTOSIZE );
CvCapture* capture = cvCreateCameraCapture(-1) ;
IplImage* frame;
while(1) {
frame = cvQueryFrame( capture );
if( !frame ) break;
cvShowImage( "Example2", frame );
char c = cvWaitKey(33);
if( c == 27 ) break;
}
cvReleaseCapture( &capture );
cvDestroyWindow( "Example2" );
return(0);
}
cvCreateCameraCapture() doesn't like CV_CAP_ANY, but seems to be happy with -1
(which is supposed to query the user for the camera to use).
Anyway, has anyone managed to get wandcam to work without gstreamer?
Ed
Ok, will this be fixed, or is there a workaround?
It's a little bit strange though, that the example here uses OpenCV for capturing: Fast GPU Image Processing in the i.MX 6x
And: Accessing an attached USB webcam works with OpenCV.
I already tried capturing the frames with gstreamer, but that didn't work with higher resolutions than PAL.