Can someone give me a WinCE7 driver for EMIF of i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can someone give me a WinCE7 driver for EMIF of i.MX53

693 Views
huachengfeng
Contributor I

Hi, guys

I'm now developing the i.MX53 system based on the Advantech ROM 1210 board. I want to use the system bus, EMIF, as the communication tool between the ARM and FPGA to transfer data. But I cannot get the WinCE7 dirver for the EMIF no matter how I try.

Can someone please kindly help me to give me the driver code for the EMIF? So many thanks!

0 Kudos
Reply
1 Reply

550 Views
igorpadykov
NXP Employee
NXP Employee

Hi HUACHENG

one can look at nxp wec7 bsp for i.MX53 smd board

Board Support Packages (10)
Windows Embedded Compact 7 BSP for i.MX53 Processor. Support SABRE
Platform for Tablets and Automotive (REV 11.05)
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

but seems it has not nor driver. In general one can develop it using
BSP Porting Guide for Windows Embedded Compact 7 from download.microsoft.com :
http://download.microsoft.com/download/2/4/A/24A36661-A629-4CE6-A615-6B2910A1367A/BSP%20Porting%20Gu...

or apply to third parties like adeneo or iwavesystems.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply