Can single i.MX6Q decode four 720p channels (MJPEG) at 30 fps?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can single i.MX6Q decode four 720p channels (MJPEG) at 30 fps?

Jump to solution
1,008 Views
DipenPatel1z
Contributor III

Dear All,

We would like to use i.MX6Q in one of our design. However we are not sure if single i.MX6Q can decode four 720p channels (MJPEG) at 30 fps?

Can anyone clarify if it is possible?

If not then what is the maximum fps that can be achieved with four 720P MJPEG channels?

Regards,

Dipen Patel

Tags (3)
1 Solution
514 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dipen

yes it can, some characteristics can be found in presentation

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
515 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dipen

yes it can, some characteristics can be found in presentation

Q&A: MX6 VPU H.264 Dual Stream Encode Limits

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
514 Views
DipenPatel1z
Contributor III

Thanks Igor.

0 Kudos