Can one of the TSN ports be configured as standard Ethernet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can one of the TSN ports be configured as standard Ethernet

393 Views
Mynxp_ravi
Contributor I

Hi,

I am looking at RT1180 feature set. I understand this processor has 4 port TSN switch with 1 TSN end point. 

I would like to use both TSN and standard Ethernet interface in my new design. Can i configure one of the four TSN ports to work as standard ethernet? Is it configurable? Please suggest.

Regards

Ravi

0 Kudos
Reply
1 Reply

372 Views
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Yes, it can be used as standard ethernet. As a TSN device would communicate with both TSN and standard ethernet. Also, TSN is an extension of standard ethernet, so I think it would work backwards.

Best regards,

0 Kudos
Reply