Can not run RPMSG pingpong demo app in imx8qxp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not run RPMSG pingpong demo app in imx8qxp

2,506 Views
nxf41732
NXP Employee
NXP Employee

Hi all,

 I am trying to run the ping-pong application on imx8qxp with core A35 run linux version 4.9.88-05083 and core M4 run RTOS version 2.5.1. 

In Uboot console I implement following below step:

- fatload mmc 1:1 0x88000000 rpmsg_lite_pingpong_rtos_linux_remote.bin

- dcache flush

- bootaux 0x88000000

(it shows log:     RPMSG Ping-Pong FreeRTOS RTOS API Demo...

                          RPMSG Share Base Addr is 0x90010000)

- boot (to boot linux console)

In Linux console I insert module:

- insmod imx_rpmsg_tty.ko

- insmod imx_rpmsg_pingpong.ko

And run 'ls /dev' command. but I don't see " ttyRPMSG " device file in "dev" folder.

Could anyone has any suggestion to fix this Issue?

Many Thanks,

Tung

0 Kudos
3 Replies

1,779 Views
angelo_d
Senior Contributor I

I had the same issue of the first question about imx8qxp.

The second question should have probably been
posted in a separate thread, since it burned the first one.

If anyone with imx8qxp will try to follow 2.8 of the above manual,
(bu bootaux) with 5.4 imx kernel, it will likely not work. M4 app will stop before
reaching Linux prompt.

The only way i had M4 app running is when it is flashed togehter
SCU firmware (see yocto imx_boot), that seems the default in last
meta-imx zeus yocto stuff.

 

0 Kudos

1,980 Views
anurag16doshi
Contributor II

I am trying to run the echo application available in the MCUExpresso SDK for the imx8mn-evk board. I compiled the application in IAR(IDE) and added the bin file to the fat32 section of my sd card. The card has a bootable Android 10.0 available for the board on the NXP website. I am using UBoot command line to run the application on the M7 core. I am receiving an output on the UART of the M7 core. I have a few questions as listed below:

1. How do I view the output of the A53 core(I have a COM terminal connected and using the Uboot command line on this terminal)?

2. Does the A53 core need to be booted for Linux in the application?

3. If no(for 3), how did you view the output while running the Android core?

4. If available can someone point me to the detailed documentation for the echo application?

0 Kudos

1,980 Views
joanxie
NXP TechSupport
NXP TechSupport

1) pls refer to the chapter 2.8 Remote Processor Messaging  and chapter 2.8.5 Running i.MX RPMsg Test Programs of enclosed file

2) you can use RPMsg application from the SDK , the SDK you can download from :

Welcome | MCUXpresso SDK Builder 

0 Kudos