Hey, I change the startup method.
I flashed the 8MM EVK BSP to the 8MM EVK board and the device was able to enter the yocto file system.
I flashed the ir_acs_live_image.img file to the USB device. After that, the USB will have two partitions
:BOOT and RESULT.
Then plug the USB device into the 8MM EVK board.
The 8MM EVK board boots up and the bootloader has found the EFI removable media binary file efi/boot/bootaa64.efi.
But the 8MM evk board still goes into the yocto file system and nothing happens.
Then 8MM evk board enter bootlader, I enter "setenv mmcdec 1" then enter "run bootcmd".
Below is my console message:
-boot=> setenv mmcdev 1
u-boot=> run bootcmd
Working FDT set to 43000000
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
starting USB...
Bus usb@32e40000: USB EHCI 1.00
scanning bus usb@32e40000 for devices... 2 USB Device(s) found
scanning usb for storage devices... 1 Storage Device(s) found
Device 0: Vendor: USB Rev: 1.00 Prod: SanDisk 3.2Gen1
Type: Removable Hard Disk
Capacity: 58680.0 MB = 57.3 GB (120176640 x 512)
... is now current device
Scanning usb 0:1...
48263 bytes read in 2 ms (23 MiB/s)
MMC: no card present
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
Found EFI removable media binary efi/boot/bootaa64.efi
647168 bytes read in 18 ms (34.3 MiB/s)
Error: Cannot initialize UEFI sub-system, r = 3
EFI LOAD FAILED: continuing...
MMC: no card present
switch to partitions #0, OK
mmc2(part 0) is current device
Scanning mmc 2:1...
48263 bytes read in 9 ms (5.1 MiB/s)
Error: Cannot initialize UEFI sub-system, r = 3
Running BSP bootcmd ...
MMC: no card present
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Can't set block device
MMC: no card present
** Bad device specification mmc 1 **
Couldn't find partition mmc 1:1
Can't set block device
Booting from net ...
ethernet@30be0000 Waiting for PHY auto negotiation to complete......................................... TIMEOUT !
Could not initialize PHY ethernet@30be0000
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17