Hello
Is i.mx 6 SoloX (MCIMX6X1AVO08AB) capable of starting with QSPI 2 - Nor - Flash boot even when USB-OTG1 and SD card are unmounted?
I wrote QuadSPI Configuration Parameters (512 B) to Nor-Flash offset value 0x400 connected to SS0 of QSPI2A1 using the J-TAG debugger, wrote u-boot-qspi2.Imx created with Yocto to offset value 0x1000 but it did not start.
BOOT_CFG[7:0] = 0x18 ([2:0]=000b,[3]=1b,[7:4]=0001b)
BOOT_CFG[15:8]=0x00
BOOT_MODE[1:0]=10b (Internal ROM Boot)
Thanks
Original Attachment has been moved to: qspi-nor-micron-n25q512a-config.zip
Hello,
Please look at the following
https://community.nxp.com/message/669485
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
Hello, Hirokata !
please check pin connection, using Table 8-27 (QSPI IOMUX pin configuration)
of the i.MX6SX RM (Rev. 1, 6/2016). Also, You may send me circuit diagram of Your design
for verifying - via request.
Regards,
Yuri.
Thanks, Yuri
Sorry, I can not send the circuit diagram to you because of the confidentiality obligation.
I tried tracing from the reset vector with the JTAG debugger.
At the address 0x0000286C of the Internal ROM, the CMP instruction is always true, so an infinite loop has been established with 0x0000286A.
What is this judgment?
Does it fail with secure boot?
Is i.MX6 SoloX able to boot without writing the program with MFG-Tool?
Can not I start up if I write directly to Flash ROM?
Regards,
Hirokata.