Can imx8mq support 256GB Micro SD Card?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can imx8mq support 256GB Micro SD Card?

Jump to solution
581 Views
传策薛
Contributor V

Hi community:

    Can someone tell me if imx8mq chip  support 256GB Micro SD Card? 

thank you !

0 Kudos
1 Solution
480 Views
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛

yes it can support it as i.MX8M uSDHC is compatible withSD/SDIO standard up to

version 3.0, MMC standard, up to version 5.0.

MultiMediaCard - Wikipedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
481 Views
igorpadykov
NXP Employee
NXP Employee

Hi 传策 薛

yes it can support it as i.MX8M uSDHC is compatible withSD/SDIO standard up to

version 3.0, MMC standard, up to version 5.0.

MultiMediaCard - Wikipedia 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------