Can imx6solo support ISL79985 ‘s 4 camera in?

cancel
Showing results for 
Search instead for 
Did you mean: 

Can imx6solo support ISL79985 ‘s 4 camera in?

626 Views
翔李
Contributor IV

HI,

Can imx6solo support ISL79985 ‘s 4 camera in?

We use intersil's isl79985-mipi to camputre 4 D1 camera video to imx6solo's 2 mipi lane,can imx6solo support?

I know IMX6Q support ISL79985 by its 4 lane,but IMX6SOLO only has 2lane and 2 virtual channel.

can imx6solo support isl79986-bt656 interface?where is the driver?

thanks.

ISL79985 datasheet is following:

ISL79985 | Video Decoders | Intersil 

pastedImage_2.png

0 Kudos
3 Replies

322 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi

attached sensor has 2 lanes which should be fine for i.MX6S.

4 cameras can be processed as in below

pastedImage_1.jpg

since i.MX6S has only two CSI (one IPU), this could not be fully implemented. Seems it could

be processed in generic format, with further processing in software. I am not aware of efforts

for developing driver for this sensor.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

322 Views
翔李
Contributor IV

HI,

  thanks a lot.

  Do you mean imx6s can not support isl79985?

  If isl79985 can mix 4camera video to one virtual channel,do imx6s can support it?

0 Kudos

322 Views
igorpadykov
NXP TechSupport
NXP TechSupport

>  If isl79985 can mix 4camera video to one virtual channel,do imx6s can support it?

yes

0 Kudos