Can i use Hynx memory and flash with imx6 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can i use Hynx memory and flash with imx6 processor

1,330 次查看
raghavendraanja
Contributor II

Hi all

i need to use the memory and flash from Hynx with part numbers

H5TQ4G63MFR-*xxC-Memory

HY27UF084G2M-Flash


Has any one used this with iMx6.


What is the reliability? i have chosen this keeping in the cost of my product.

标签 (1)
0 项奖励
回复
2 回复数

1,126 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

hello,raghavendra,

       Please send their datasheets to me ! Let me check them . My email : weidong.sun@freescale.com

Thanks,

Weidong

0 项奖励
回复

1,126 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

hello,raghavendra,

      I checked the datasheets of memory and nand flash, They are both OK for i.mx6. Only please note DDR3 memory capacity, on MX6 EVK, it is 2Gbit, yours is 4Gbit, So software engineer will re-configure u-boot/board/freescale/mach-mx6q/flash_header.S, which is configure memory controller . Reference document is Reference manual.

Regards,

Weidong

0 项奖励
回复