Hi all,
I saw below message below at iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP :
The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.
The 4 cameras can be:
- 1xCSI, 3xMIPI
- 2xCSI, 2xMIPI
- 4xMIPI
it supports 4XD1 video
But in my case ,i need it supports 3XD1 and 1X720P cameras input at the same time.
then ,Can i use 1xCSI, 3xMIPI ?1 csi for 720p and 3XMIPI for D1?
can it work at the same time?
TKS
Hi
in general yes, it is possible to use use 1xCSI, 3xMIPI ?1 csi for
720p and 3XMIPI for D1 at the same time.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------