Can i install Ubuntu for imx7 Sabre board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i install Ubuntu for imx7 Sabre board?

2,082 Views
atakanakbulut
Contributor II

Hello everyone im trying for install Ubuntu for imx7d sabre board is it possible? I created distro via yocto but its not usable. I want to install Ubuntu Kubuntu or deb based ready Distros . one topic has a for imx6 but i could not see for imx7. 

Thank you 

0 Kudos
Reply
1 Reply

1,472 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Atakan,

Ubuntu is not oficially supported by NXP but the following link may help.

Installing Ubuntu Rootfs on NXP i.MX6 boards 


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply