Can i have example source for EMIF(External memory interface) function?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can i have example source for EMIF(External memory interface) function?

1,890 次查看
hanseunglee
Contributor III

I check i.mx6dl interface for data transfer from fpga chip.

so.. if i.mx6 sabresd board can use EMIF function, can i have example code or manual?

I already search unit_test example folder but i can not find EMIF file.

If you know every information about EMIF, reply please.

标签 (4)
0 项奖励
回复
2 回复数

1,624 次查看
ruiguo
Contributor II

Hi Hanseung

I am glad to read your article for EIM and FPGA.I am studying them in our work. But I meet a hard problem that the signal is not produced in the EIM bus. I hope you can help me to share your code. sincerely! I look forward to your replay.

Rui

0 项奖励
回复

1,624 次查看
art
NXP Employee
NXP Employee

The i.MX6DualLite processor has many various interfaces to receive data from FPGA. Those are the parallel External Memory Interface Module (EIM, primarily meant for connection of an external SRAM/NOR Flash like memories), parallel Camera Sensor Interface (CSI) that allows raw data transfer to memory, PCIe (if supported by FPGA). The particular connection method is FPGA-dependent.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复