Can i.MX8 QM HDMI_TX pull-down resistor 604Ω be changed?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX8 QM HDMI_TX pull-down resistor 604Ω be changed?

394 Views
DITTO
Contributor I

In the《 i.MX8 QM / i.MX8 QXP Hardware Developer’s Guide》file,For the HDMI output, note that there are 604 Ω resistors on the positive and negative sides of each high-speed output pair that are grounded through a FET;Can Replace the  604 Ω resistor  with other values? Is there more detailed information available?   Thanks!

0 Kudos
Reply
1 Reply

387 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please refer the Hardware Developer’s Guide.Don't replace this 604 Ω resistors

This is the optimum value for stable HDMI operation

0 Kudos
Reply