Can i.MX6SL support 1.8v DDR2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX6SL support 1.8v DDR2?

Jump to solution
680 Views
JHY
Contributor IV

Hi,

Below is from IMX6SLCEC.pdf.

It says i.MX6SL supports DDR3, LVDDR3, LPDDR2.

Maybe not, I want to confirm whether it supports 1.8V DDR2 or not.

Best regards.

Labels (1)
Tags (1)
0 Kudos
1 Solution
642 Views
Yuri
NXP Employee
NXP Employee

  Alas, the i.MX6 does not support the DDR2.

Have a great day,
Yuri
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
643 Views
Yuri
NXP Employee
NXP Employee

  Alas, the i.MX6 does not support the DDR2.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos