Can i.MX6 boot with no attached DDR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX6 boot with no attached DDR?

897 Views
michaeln
Contributor I

Hi Everyone,

Newbie here.  My team has asked if an i.MX6 can boot with no DDR attached,

and I'm having problems finding the info in any of the documents.

Thanks,

Mike

Labels (1)
0 Kudos
Reply
1 Reply

828 Views
Yuri
NXP Employee
NXP Employee

Hello,

  it is possible to load / boot and run relatively simple application to internal

memory (OCRAM) of the i.MX6 without external DDR.

Please look at an example, attached in the following thread.

Integrating Processor Expert for i.MX and ARM GCC with Eclipse


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply