Can i.MX6 IPU SMFC use multiple DMA channel if image data inputs from parallel camera?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can i.MX6 IPU SMFC use multiple DMA channel if image data inputs from parallel camera?

跳至解决方案
1,649 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6Q IPU.

Please see Figure 37-22 in IMX6DQRM Rev.1.

According to this figure, SMFC has 4 DMA channels.

And SMFC seems that it can use multiple channels to transfer data input from MIPI-CSI.

Then, how about in the case input from parallel camera?

Can SMFC use only one DMA channel to transfer if data is input from a parallel camera?

Or can it use multiple DMA channels?

Best Regards,

Satoshi Shimoda

标签 (4)
标记 (2)
0 项奖励
回复
1 解答
1,383 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

you are right, from a parallel camera SMFC can use

only one DMA channel. "DI (data identifier)" concept is used

only for MIPI interface, this is described in sect.37.4.3.2.2

IMX6DQRM  i.MX 6Dual/6Quad Applications Processor Reference Manual

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,384 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi,

you are right, from a parallel camera SMFC can use

only one DMA channel. "DI (data identifier)" concept is used

only for MIPI interface, this is described in sect.37.4.3.2.2

IMX6DQRM  i.MX 6Dual/6Quad Applications Processor Reference Manual

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复