Can i Boot imx8mq with out uboot/linux/android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i Boot imx8mq with out uboot/linux/android

1,764 Views
shangregister
Contributor II

hi all

Can i Boot imx8mq without uboot or linux/android?

Just boot a small fimware for controller.

Hanson

Labels (1)
0 Kudos
Reply
5 Replies

1,663 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hanson

in general (unfortunately nxp does not provide such examples) it is possible, for example

setting application ivt addresses to On-Chip RAM - OCRAM, described in

Figure 6-18. Image Vector Table i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

AN12107 in sect.2.5.1 IVT data structure gives more detailed description of ivt usage

https://www.nxp.com/docs/en/application-note/AN12107.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,663 Views
shangregister
Contributor II

i saw the DDR tools has a firmware ,and that firmware did not use the uboot to bootup imx8mq.

how can i compile that firmware?

0 Kudos
Reply

1,663 Views
igorpadykov
NXP Employee
NXP Employee

sources of that firmware are not available for customers.

In general it uses the same concept as suggested above.

Best regards
igor

0 Kudos
Reply

1,663 Views
shangregister
Contributor II

So Did any compiler or ide is provided by nxp can doing this?

0 Kudos
Reply

1,663 Views
igorpadykov
NXP Employee
NXP Employee

this does not depend on compiler or ide, it is necessary to write custom

application for that.

Best regards
igor

0 Kudos
Reply