Can-bus on NXP i.MX7D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can-bus on NXP i.MX7D

793 Views
andreasaccomand
Contributor I

I need to use the can-bus on 'NXP i.MX7D' in androidthings, I only found the documentation of the connectors, but absolutely nothing about how to software interface. It is possible to activate the can0 or I have to drive directly the can controller ?
Andrea

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

680 Views
andreasaccomand
Contributor I

I am using PICO-PI-IMX7,

precisely this:

NXP i.MX7D  |  Android Things  |  Android Developers 

with:

Android 8.1.0  API Level 27

Thank you very much

Andrea

0 Kudos
Reply

680 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Andrea,

The PICO-PI-IMX7 is the third party design board, I have searched and find few materials about it. Here I recommend you to refer to our NXP linux BSP FlexCAN driver,  drivers/net/can/flexcan.c. You can try to add it to your kernel. Hope this can do help for you.

Have a nice day

Rita

0 Kudos
Reply

680 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board and BSP are you using?

0 Kudos
Reply