Hi All
I am planning to use NXP MCIMX7D5EVM10SD product, I have a problem in using DDR3.
Our plan is to use DDR3 16-bit single.
I would like to know if you can use 16-bit DDR3 as a single in the i.MX7D and if it is available, what are the requirements?
Hi Kenneth
16 bit ddr can be used by selection of DATA_BUS_WIDTH field DDRC_MSTR register as
described in sect.9.2.5.2.1 Master Register (DDRC_MSTR) i.MX7D Reference Manual
http://cache.nxp.com/files/32bit/doc/ref_manual/IMX7DRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------