Can SSD be used with IMX536?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can SSD be used with IMX536?

Jump to solution
646 Views
varunsharma
Contributor I

Hello,

We are using IMX536 in our design and also we are using Solid state drive (SSD).

IMX536 datasheet specifies SATA HDD interface.

So my question is:

Can i use SATA SSD with HDD interface?

Also, let us know the availability of driver

Plz let us know if we are missing something.

Thanks in advance!!

Labels (1)
Tags (1)
0 Kudos
1 Solution
546 Views
SergioSolis
NXP Employee
NXP Employee

Hello Varun,


The i.MX53 supports boot from HD and SSD devices using the PATA and SATA interfaces.

Please take a look at section 7.5.4 in the i.MX53 Reference Manual for more information on SSD configuration.

View solution in original post

0 Kudos
1 Reply
547 Views
SergioSolis
NXP Employee
NXP Employee

Hello Varun,


The i.MX53 supports boot from HD and SSD devices using the PATA and SATA interfaces.

Please take a look at section 7.5.4 in the i.MX53 Reference Manual for more information on SSD configuration.

0 Kudos