Can MX8QM support duplicate outputs on two LVDS displays?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can MX8QM support duplicate outputs on two LVDS displays?

1,411 次查看
RobbieJiang
Contributor IV


We have a MX8QM board (with Yocto BSP 4.19.35) with two LVDS outputs( LVDS-1 and LVDS-2),
both with the same resolution 800x480@30fps.

And the application needs to output duplicate content on these two different LVDS displays.

On MX6Q, output LVDS ports can be used as:
"Two identical outputs: single input sent to both output channels".
This is exactly what we need.

Can MX8QM LVDS output ports support the same mode ?

If not, how can I get two different LVDS displays to output the same content on MX8QM SoC?

 

Regards,

Robbie

0 项奖励
回复
2 回复数

1,401 次查看
RobbieJiang
Contributor IV
0 项奖励
回复

1,393 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes you can refer to this

0 项奖励
回复