Can MX8QM support duplicate outputs on two LVDS displays?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can MX8QM support duplicate outputs on two LVDS displays?

1,445 Views
RobbieJiang
Contributor IV


We have a MX8QM board (with Yocto BSP 4.19.35) with two LVDS outputs( LVDS-1 and LVDS-2),
both with the same resolution 800x480@30fps.

And the application needs to output duplicate content on these two different LVDS displays.

On MX6Q, output LVDS ports can be used as:
"Two identical outputs: single input sent to both output channels".
This is exactly what we need.

Can MX8QM LVDS output ports support the same mode ?

If not, how can I get two different LVDS displays to output the same content on MX8QM SoC?

 

Regards,

Robbie

0 Kudos
Reply
2 Replies

1,435 Views
RobbieJiang
Contributor IV
0 Kudos
Reply

1,427 Views
joanxie
NXP TechSupport
NXP TechSupport

yes you can refer to this

0 Kudos
Reply