Can Linaro Android v4.0.4 (release 12.05) be easily configured to use QSB 4.3 inch LCD/touchscreen?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Linaro Android v4.0.4 (release 12.05) be easily configured to use QSB 4.3 inch LCD/touchscreen?

513 Views
RobThompson
Contributor I

Hi all,

I would like to use the current Linaro Android image for the Freescale QSB with the 4.3 inch (i.mx28) LCD/touchscreen offered for the QSB.  Using the prebuilt image, the QSB drives the VGA interface by default.  Our Android programmers want to use several of the features found in Android v4.0.4 (ICS) that are not available in the Adeneo Android v2.3 (Gingerbread) image.

Is there a set of u-boot assignments (i.e., video=LCD, etc.) that would configure the QSB to use the LCD and touchscreen and, if so, what are the details?

Any information or references would be helpful.

Thanks

Labels (1)
0 Kudos
Reply
0 Replies