Can IMX6 fix the sample rate before output from I2S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can IMX6 fix the sample rate before output from I2S

785件の閲覧回数
jane-jiajuan_zh
Contributor III

Hi, 

My board use imx6solo, and the codec chipset is only support the 8K sample rate. so we hope to fix the sample rate before IMX6 output from I2S.

We tried gstreamer re-sample pipeline, and it works. But we hope to find a hardware way to support it.

Is that possible by any hardware module to fix the sample rate?

Best Regards,

Jane

0 件の賞賛
返信
1 返信

750件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jane

i.MX6Q has ASRC module for such purpose, so one can check ASRC driver description

in Linux Manual included in Linux 4.19.35_1.1.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信