Can IMX515 output BT656/1102 in 24-bit from DI0 or DI1 parallel interface? And I need 8 bit BT.656 signal connnet to IMX6D CSI interface .
Hi ming
yes it can, but only up to 16 bit, from MCIMX51RM sect.42.1.3.1.2 Display Ports,
The Interface:
The following interface types are provided (in each of the two display ports)
• Parallel video interface (for synchronous access) - up to 24-bit data bus.
— Control protocol - follows Sharp HR and generic TFT definitions
— Supports BT.656 (8-bit) and BT.1120 (16-bit) protocols
no problems with 8 bit BT.656 signal connnection to IMX6D CSI interface.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
thanks for your repay , but what I need was Patch to Support BT656 and BT1120 Output For i.MX515 BSP .