Can IMX515 output BT656/1102 in 24-bit DI0 or DI1 parallel interface?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can IMX515 output BT656/1102 in 24-bit DI0 or DI1 parallel interface?

1,256 Views
36766362
Contributor I

Can  IMX515 output BT656/1102 in 24-bit from  DI0 or DI1  parallel interface?   And  I need  8 bit BT.656 signal connnet to   IMX6D CSI interface .

Labels (1)
0 Kudos
3 Replies

1,153 Views
igorpadykov
NXP Employee
NXP Employee

Hi ming

yes it can, but only up to 16 bit, from MCIMX51RM sect.42.1.3.1.2 Display Ports,

The Interface:

The following interface types are provided (in each of the two display ports)

• Parallel video interface (for synchronous access) - up to 24-bit data bus.

— Control protocol - follows Sharp HR and generic TFT definitions

— Supports BT.656 (8-bit) and BT.1120 (16-bit) protocols


no problems with 8 bit BT.656 signal connnection to IMX6D CSI interface.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,153 Views
36766362
Contributor I

Hi igorpadykov,

  thanks for your repay  ,   but what I need was  Patch to Support BT656 and BT1120 Output For i.MX515 BSP .

0 Kudos

1,153 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos