Can I use two displays(HDMI + LCD) at the same time to display two usb camera inputs?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use two displays(HDMI + LCD) at the same time to display two usb camera inputs?

522 次查看
mckim
Contributor I

Hello,

Can I use two displays(HDMI + LCD) at the same time to display two usb camera inputs and GUI on i.MX8MQ?

I would like to show one usb camera input with GUI on one display(HDMI), and
show the other usb camera input with GUI on the other display(LCD)?

Other post in this forum said one display show only video and the other display shows only GUI, Is this true?
after checking i.MX Reference Manual, I think there is a possibility for what I want,
because two GUIs can be displayed on both HDMI and LCD, and
two usb camera inputs is not processed as video(I think this is processed like GUI, even though it will be processed with gstreamer).
But I am not sure.

Could you let this issue clear?

Thank you in advance.

 

标签 (1)
0 项奖励
回复
2 回复数

519 次查看
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX Linux User’s Guide​, Chapter 7.3.1.6.1, I think it is possible to display two different inputs to two different displays.

0 项奖励
回复

514 次查看
mckim
Contributor I

Hello, Jimmychan,

Thank you for the reply,

but Could you answer it more cleary?

on the document, i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual, the section 13.1.1.1, it says,

The following use cases are supported:
• Dual display: HDMI driven by Display Controller, with video playback support on
HDMI; MIPI driven by LCDIF, without video playback support on MIPI
• Single display: HDMI driven by Display Controller, with video playback support on
HDMI
• Single display: MIPI driven by Display Controller, with video playback support on
MIPI
• Single display: MIPI driven by LCDIF, without video playback support on MIPI.

I am very confusing and I am not sure i.MX8MQ can support what i want.

 

Could you answer it for sure?

 

Thank you...

0 项奖励
回复