Can I use the device sai in the user space?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use the device sai in the user space?

860 次查看
delauratfrançoi
Contributor II


Hello,

My name is françois. I work with imxd7. In my personnal board I have Bluetooth module. The bluetooth module is conneted with imxd7 by uart and sai port. I do not know how to use the sai port with the bluetooth module. I saw the example with sound card but it's not the same thing.

Have you got an example.

Can I use the device sai in the user space.

What should I write in device tree.

Thanks for All Help.

Best regards,

François.

标签 (3)
0 项奖励
回复
1 回复

672 次查看
igorpadykov
NXP Employee
NXP Employee

Hi François

I am not aware of such ways and think that it is necessary to

write application based on sai driver, please refer to attached Linux

Manual sect.28.4.1 ASoC Driver Source Architecture. As example one

can look at Chapter 55 Bluetooth driver.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复