Can I use the Vivante closed-source driver for an RTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use the Vivante closed-source driver for an RTOS

916件の閲覧回数
bastian_schick
Contributor IV

Hi,

did someone try to use the Vivante driver with an RTOS? How much of "Linux" does the driver need to work?

ラベル(3)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

687件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello 42Bastian,

The Vivante driver it is completely based for Linux,  so it can not be used as binary in other operating Systems.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

687件の閲覧回数
bastian_schick
Contributor IV

The question is: What does it need from Linux?

Of course the other question: Why isn't there a baremetal version of the library?

0 件の賞賛
返信