Can I use the Vivante closed-source driver for an RTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the Vivante closed-source driver for an RTOS

950 Views
bastian_schick
Contributor IV

Hi,

did someone try to use the Vivante driver with an RTOS? How much of "Linux" does the driver need to work?

Labels (3)
Tags (1)
0 Kudos
Reply
2 Replies

721 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello 42Bastian,

The Vivante driver it is completely based for Linux,  so it can not be used as binary in other operating Systems.


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

721 Views
bastian_schick
Contributor IV

The question is: What does it need from Linux?

Of course the other question: Why isn't there a baremetal version of the library?

0 Kudos
Reply