Can I use the Kobs-ng command to change bootstreams

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the Kobs-ng command to change bootstreams

1,050 Views
yongban
Contributor II

Can I use the Kobs-ng command to change bootstreams?(可以用Kobs-ng命令改bootstreams吗?)

Labels (1)
0 Kudos
Reply
1 Reply

970 Views
art
NXP Employee
NXP Employee

You can use the kobs-ng tool to program various boot images to NAND Flash memory.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply