Can I use sb_loader load u-boot and uImage to Ram.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I use sb_loader load u-boot and uImage to Ram.

ソリューションへジャンプ
965件の閲覧回数
geekdarcy
Contributor III

hi,all

I'm developing a new board based on the IMX6Q.

I had load u-boot.bin to ram , it run successfully.

Meanwhile,can i load my custom uImage to Ram by sb_loader.

I had try to do that,the step is as follws:

->sb_loader -nojump -f 

->sb_loader -trans 0x10800000 -f uImage
->sb_loader -exec 0x27800000

Any clue about the question?
ラベル(2)
1 解決策
784件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

please look at sb_loader usage

i.MX USB Loader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
785件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi li

please look at sb_loader usage

i.MX USB Loader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------