Can I use I.mx6ull GPIO2_IO11 pin A15 as a interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use I.mx6ull GPIO2_IO11 pin A15 as a interrupt

Jump to solution
755 Views
prabhu1
Contributor III

Hi, Can you give info on GPIOs and Interrupt pins details.

In my design, I am using GPIO2_IO11 pin A15 as an interrupt in i.mx6ull.

So can I use that GPIO pin as an interrupt pin?

1 Solution
696 Views
igorpadykov
NXP Employee
NXP Employee

Hi prabhu

any gpio can be used as interrupt source, some examples can be found on

Configured GPIO interrupt but ISR is not hitting 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
697 Views
igorpadykov
NXP Employee
NXP Employee

Hi prabhu

any gpio can be used as interrupt source, some examples can be found on

Configured GPIO interrupt but ISR is not hitting 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

696 Views
prabhu1
Contributor III

Hi Igorpadykov,

Thanks for your help.

0 Kudos