Can I remove diode between P3V0_VSNVS and P3V15_VDDHIGH ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I remove diode between P3V0_VSNVS and P3V15_VDDHIGH ?

跳至解决方案
1,168 次查看
ko-hey
Senior Contributor II

Hi all 

I have a question about connecting diode between VDD_SNVS_IN and VDD_HIGH_IN.

I'm referring a iMX6SLEVK_DESIGNFILES/Schematics/spf-27452_b.pdf.

According to the schematic, there is a diode between VDD_SNVS_IN and VDD_HIGH_IN as below.

pastedImage_1.png

My customer are trying to reduce the number of parts as they as possible. 

When they don't use RTC, can they remove the diode ?

Ko-hey

标签 (4)
0 项奖励
回复
1 解答
980 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Some current flow can take place between i.MX6 VDD_SNVS_IN and  VDD_HIGH_IN, when they

are not equal. Therefore it is recommended that voltage difference between these pins should not

exceed 0.3V  to avoid high current leakage.

  VDD_HIGH_IN and VDD_SNVS_IN can be tied together if the real-time clock function is not
needed during system power-down.

 

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
981 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Some current flow can take place between i.MX6 VDD_SNVS_IN and  VDD_HIGH_IN, when they

are not equal. Therefore it is recommended that voltage difference between these pins should not

exceed 0.3V  to avoid high current leakage.

  VDD_HIGH_IN and VDD_SNVS_IN can be tied together if the real-time clock function is not
needed during system power-down.

 

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
980 次查看
ko-hey
Senior Contributor II

Hi Yuri Muhin

As a result, user can remove a diode if they want to.

NXP recommends that voltage difference between these pins should not exceed 0.3V to avoid high current leakage when user remove diode.

Am I correct ?

Ko-hey

0 项奖励
回复
980 次查看
Yuri
NXP Employee
NXP Employee

  You are correct; perhaps it would be better just to connect  together 

VDD_HIGH_IN and VDD_SNVS_IN.

Regards,

Yuri.