Can I leave RESETN of i.MX28 floating?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I leave RESETN of i.MX28 floating?

Jump to solution
1,076 Views
hikaruuruno
Contributor III

Hello all,

We are designing a board using i.MX280 and there is a question we'd like to ask.

There is a description that RESETN does not need external pull up on the page 11, IMX28CEC.

The question is, as mentioned as a title, can I leave the pin floating without a capacitor?

Or should I place a capacitor to the RESETN pin?

Usually, when we design a circuit, we place a capacitor to a reset pin, so floating reset pin looks weird.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
971 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

yes one can leave the pin floating without a capacitor,

no any external connection of this pin is required if not used.

Floating reset pin will not cause problems since it resets the chip if it

is low for more than 100ms, it has internal pull-up and chip reset is provided

by other signals (PSWITCH or connection to VDD5V).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
972 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

yes one can leave the pin floating without a capacitor,

no any external connection of this pin is required if not used.

Floating reset pin will not cause problems since it resets the chip if it

is low for more than 100ms, it has internal pull-up and chip reset is provided

by other signals (PSWITCH or connection to VDD5V).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
971 Views
hikaruuruno
Contributor III

Hi Igor,

Thank you for the answer.

We'll leave the pin floating.

Best regards,

Hikaru

0 Kudos
Reply