Can Cortex-M4 core use OCRAM without conflicting by linux or u-boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can Cortex-M4 core use OCRAM without conflicting by linux or u-boot?

跳至解决方案
1,929 次查看
Takashi_Kashiwagi
Senior Contributor I

Hi Community.

I'm making a program for the CM4 core. I would like to use OCRAM because TCM seems to lack capacity.

I think that linux doesn't seem to use OCRAM, but I didn't know if u-boot was using it.

Does anyone know how OCRAM is used by u-boot and linux?

(It is good for me that OCRAM is only used by BootROM.)

Best Regrads,

T.Kashiwagi

标记 (3)
0 项奖励
回复
1 解答
1,757 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kashiwagi,

You could refer to U-Boot source code to determinate on which memory is running. On i.MX8M series, it was also included the use of the SPL, so, it may be required to also consider this. The following thread seems to be related:

Building SPL/u-boot to boot from SD on i.MX 8M QUAD EVK 

Also, SPL is described on the link below, you could use it as reference:

http://trac.gateworks.com/wiki/ventana/bootloader

Additionally, in case of lacking capacity of the TCM, the M4 core could also run from DRAM; please refer to chapter 6 of “Getting Started with MCUXpresso SDK i.MX 8M Devices” document.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,758 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi Kashiwagi,

You could refer to U-Boot source code to determinate on which memory is running. On i.MX8M series, it was also included the use of the SPL, so, it may be required to also consider this. The following thread seems to be related:

Building SPL/u-boot to boot from SD on i.MX 8M QUAD EVK 

Also, SPL is described on the link below, you could use it as reference:

http://trac.gateworks.com/wiki/ventana/bootloader

Additionally, in case of lacking capacity of the TCM, the M4 core could also run from DRAM; please refer to chapter 6 of “Getting Started with MCUXpresso SDK i.MX 8M Devices” document.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复
1,757 次查看
Takashi_Kashiwagi
Senior Contributor I

Hi Carlos-san

Thank you for responding.

Thank you for the material. I will try it.

The background, we will use CM4 core for monitoring Linux (CA53 Core).

So, I don't want to use the DRAM area as much as possible.

Because I think that DRAM is initialized by DCD and u-boot.

Best Regards,

T.Kashiwagi

0 项奖励
回复