Can Cortex-M4 core use OCRAM without conflicting by linux or u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can Cortex-M4 core use OCRAM without conflicting by linux or u-boot?

Jump to solution
868 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Community.

I'm making a program for the CM4 core. I would like to use OCRAM because TCM seems to lack capacity.

I think that linux doesn't seem to use OCRAM, but I didn't know if u-boot was using it.

Does anyone know how OCRAM is used by u-boot and linux?

(It is good for me that OCRAM is only used by BootROM.)

Best Regrads,

T.Kashiwagi

Tags (3)
0 Kudos
1 Solution
701 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kashiwagi,

You could refer to U-Boot source code to determinate on which memory is running. On i.MX8M series, it was also included the use of the SPL, so, it may be required to also consider this. The following thread seems to be related:

Building SPL/u-boot to boot from SD on i.MX 8M QUAD EVK 

Also, SPL is described on the link below, you could use it as reference:

http://trac.gateworks.com/wiki/ventana/bootloader

Additionally, in case of lacking capacity of the TCM, the M4 core could also run from DRAM; please refer to chapter 6 of “Getting Started with MCUXpresso SDK i.MX 8M Devices” document.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
702 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Kashiwagi,

You could refer to U-Boot source code to determinate on which memory is running. On i.MX8M series, it was also included the use of the SPL, so, it may be required to also consider this. The following thread seems to be related:

Building SPL/u-boot to boot from SD on i.MX 8M QUAD EVK 

Also, SPL is described on the link below, you could use it as reference:

http://trac.gateworks.com/wiki/ventana/bootloader

Additionally, in case of lacking capacity of the TCM, the M4 core could also run from DRAM; please refer to chapter 6 of “Getting Started with MCUXpresso SDK i.MX 8M Devices” document.

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
701 Views
Takashi_Kashiwagi
Senior Contributor I

Hi Carlos-san

Thank you for responding.

Thank you for the material. I will try it.

The background, we will use CM4 core for monitoring Linux (CA53 Core).

So, I don't want to use the DRAM area as much as possible.

Because I think that DRAM is initialized by DCD and u-boot.

Best Regards,

T.Kashiwagi

0 Kudos