Can ADC of i.MX25 touch screen controller be used for general purpose ADC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can ADC of i.MX25 touch screen controller be used for general purpose ADC?

1,307件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Hello,

I found below comment from i.MX25 RM, Chapter 44. Touch Screen Controller (TSC) and Analog-to-Digital Converter (ADC).

Supports general-purpose analog measurements (such as temperature and voltage) with three input channels (aux0, aux1, aux2), or 8 input channels if touch interface is not used.

So I believe ADC channel for TSC can be used for general purpose ADC but is there any body who can confirm it? If there is any limitation to use for this purpose, please let me know.

Best regards,

Paul

ラベル(2)
0 件の賞賛
返信
1 返信

1,118件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please look at AN3948 i.MX25 Integrated Analog-to-Digital Converter

http://cache.freescale.com/files/dsp/doc/app_note/AN3948.pdf?fpsp=1

0 件の賞賛
返信