Can ADC of i.MX25 touch screen controller be used for general purpose ADC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can ADC of i.MX25 touch screen controller be used for general purpose ADC?

1,349 Views
Paul_Kang
NXP Employee
NXP Employee

Hello,

I found below comment from i.MX25 RM, Chapter 44. Touch Screen Controller (TSC) and Analog-to-Digital Converter (ADC).

Supports general-purpose analog measurements (such as temperature and voltage) with three input channels (aux0, aux1, aux2), or 8 input channels if touch interface is not used.

So I believe ADC channel for TSC can be used for general purpose ADC but is there any body who can confirm it? If there is any limitation to use for this purpose, please let me know.

Best regards,

Paul

Labels (2)
0 Kudos
Reply
1 Reply

1,160 Views
Yuri
NXP Employee
NXP Employee

Please look at AN3948 i.MX25 Integrated Analog-to-Digital Converter

http://cache.freescale.com/files/dsp/doc/app_note/AN3948.pdf?fpsp=1

0 Kudos
Reply