Hi ,
I am working over the IMX6 solo , Can i interface 128MB(bytes) serial NOR Flash( SPI based) with the IMX6 solo.
As per the reference manual , BOOT_CFG4[3] Fuse , it maximum support 3 byte addressing (24-bit) .
Please advice.
Regards,
Aditya Nagal
Hi Aditya
if spi-nor supports addressing provided by BOOT_CFG4[3] Fuse,
one can boot from it, then use custom driver to use addressing protocol
supported by that nor to access full 128MB.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------